MCTPTX1AK324_Triple_PMSM_RDB code build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCTPTX1AK324_Triple_PMSM_RDB code build error

1,961件の閲覧回数
June6
Contributor I

Hello 

I just started using the development board MCTPTX1AK324 for product debugging and There are some errors while building the software MCTPTX1AK324_Triple_PMSM_RDB. pls see below picture. 

June6_0-1722911284250.png

The version of the IDE : S32DS v3.5.
The RTD pack is: S32K3 RTD AUTOSAR R21-11 Version 4.0.0. P16

IPCF : SW32K3 IPCF 4.1.0 D2312
The development package is the: S32K3xx development package version 3.5.13

The configuration of the project is shown in below images

Could you please help me check these errors?

Thank you in advance1.png2.png3.png4.png5.png

 

 

0 件の賞賛
返信
4 返答(返信)

1,942件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

After installing MCTPTX1AK324-SW.exe, the MCTPTX1AK324_ReleaseNotes.txt mentions:
Examples based on the RTD low level API(applpostfix _ll):
- S32 Design Studio for S32 Platform Version 3.5
- S32K3xx development package version 3.5.2
- S32K3 RTD AUTOSAR 4.4 Version 2.0.0 (S32DS Extesnion and Updates installation)
- FreeMASTER 3.2.1.6

Please refer to Getting Started with the MCTPTX1AK324 Evaluation Board to install S32DS v3.4 + S32K3 RTD 2.0.0 + IPCF 3.6.0.

Before installing

2.0.0   S32K3 Real Time Drivers Version 2.0.0

, please complete the installation

3.4.3_D2205   S32 Design Studio for S32 Platform v.3.4 Service Pack 4 with support for S32K341 device

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,935件の閲覧回数
June6
Contributor I

Hello Robin

Thank you for your kind reply.

When I download the IPCF3.6.0,I can not find this version, only V3.7.0. in product list. Pls see below picture. How can I get the 3.6.0? If you could share the link with me, that would be even better. Thank you.

June6_0-1722930472299.png

 

0 件の賞賛
返信

1,930件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please click Previous:

S32K3 IPCF 3.6.0.png

0 件の賞賛
返信

1,926件の閲覧回数
June6
Contributor I

June6_0-1722931587170.png

 

0 件の賞賛
返信