MCSXTE2BK142 single shunt code can't work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCSXTE2BK142 single shunt code can't work

跳至解决方案
3,646 次查看
peter_shi
Contributor II
MCSXTE2BK142\sw\MCSXTE2BK142_PMSM_FOC_1Sh
0 项奖励
回复
1 解答
3,552 次查看
jianqiuhu
NXP Employee
NXP Employee

Hi Peter,

1. you are right, the ADC channel should be modified to CH15.

2. could you remove the interrupt control INT_SYS_DisableIRQGlobal(); and INT_SYS_EnableIRQGlobal(); in function ADC0_IRQHandler(). and try again? I think the FTM3 overflow IRQ routine was delayed by the ADC0 IRQ routine.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,616 次查看
peter_shi
Contributor II

Hi,

I bought 1 pcs MCSXTE2BK142 demo board from your Website and download the demo code from the website as well.

When I used the two-shunt resistance, the function is ok. I could run motors. 

For the single-shunt demo code, I removed C68, C70, and C65 to check the function.  VF function is ok. But when I used sensor-less control, the motor can't run even if it was in open loop stage.

I checked the demo code about ADC configuration, I found the ADC configuration was wrong. The demo code used CH8, but Hardware used CH15.

I reconfigured the ADC channel, but it still doesn't work. FreeMaster report phase over current. I think dc-current sampling has some issue.

 

0 项奖励
回复
3,376 次查看
Shrikant1
Contributor I

i am not able to run it in dual shunt specifically in closed loop. Have you tried with sensoed or sensor less which type of sensor you have used.

0 项奖励
回复
3,553 次查看
jianqiuhu
NXP Employee
NXP Employee

Hi Peter,

1. you are right, the ADC channel should be modified to CH15.

2. could you remove the interrupt control INT_SYS_DisableIRQGlobal(); and INT_SYS_EnableIRQGlobal(); in function ADC0_IRQHandler(). and try again? I think the FTM3 overflow IRQ routine was delayed by the ADC0 IRQ routine.

0 项奖励
回复
3,562 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @peter_shi,

I'm sorry for the delay.

It looks like you are right, but the issue is still under investigation.

 

BR, Daniel

0 项奖励
回复
3,624 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @peter_shi,

Can you be more specific?

What error does the FreeMaster report?

 

BR, Daniel

0 项奖励
回复