MCSPTEAK116 Motor Overcurrent continuous Fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCSPTEAK116 Motor Overcurrent continuous Fault

ソリューションへジャンプ
2,411件の閲覧回数
hns80
Senior Contributor I

I am trying to run the MCSPTE1AK116_PMSM_FOC_1Sh example on the S32K116 EVK and MOTOR-GD daughterboard. I was able to build the code and run it on the micro through the debugger.

When I run FreeMaster, the OverPhaseACurrent fault gets set immediately. This occurs even if I disconnect the motor completely from the board.

hns80_0-1696281453533.png

When I stop FreeMaster and enter the debugger, I see this fault getting set.

Is there some setting that needs to change before building the code?

 

0 件の賞賛
返信
1 解決策
2,391件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

have you set boards jumper properly on boards and also set overcurrent potentiometer as Get started guide mentions?
https://www.nxp.com/document/guide/get-started-with-the-mcspte1ak116:GS-MCSPTE1AK116?section=plug-it...

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,392件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

have you set boards jumper properly on boards and also set overcurrent potentiometer as Get started guide mentions?
https://www.nxp.com/document/guide/get-started-with-the-mcspte1ak116:GS-MCSPTE1AK116?section=plug-it...

BR, Petr

0 件の賞賛
返信
2,364件の閲覧回数
hns80
Senior Contributor I

I was missing J15. After inserting it, I could at least start the motor.

That leads me to a new problem, though I will start a different thread for that.

 

0 件の賞賛
返信