MCSPTE1AK144_PMSM_FOC_1Sh Compilation failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCSPTE1AK144_PMSM_FOC_1Sh Compilation failed

2,263 Views
zhouqichen
Contributor I

hello, when compile  Official routine MCSPTE1AK144_PMSM_FOC_1Sh engineering prompt 

Description Resource Path Location Type

SDK Id=S32K14x_AMMCLIB_1.1.18_PATH for the Project "MCSPTE1AK144_PMSM_FOC_1Sh" is not found in SDKs list! Ignored. MCSPTE1AK144_PMSM_FOC_1Sh P/MCSPTE1AK144_PMSM_FOC_1Sh Missed SDK Marker 

Description Resource Path Location Type
ERROR: Retrieving SDK version failed, please check SDK source files consistency (D:\NXP\S32DS_ARM_v2018.R1\eclipse\ProcessorExpert/../../S32DS/software/S32SDK_S32K1xx_RTM_3.0.0*manifest.xml not found or corrupted). MCSPTE1AK144_PMSM_FOC_1Sh Cpu Processor Expert Problem

 

current software:S32DS_ARM_Win32_v2018.R1_b180326   S32DS_ARM_v2018.R1_UP11.zip ,Which version should I download

0 Kudos
Reply
3 Replies

2,242 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi zhouqichen,

Please try to use software shown in MCSPTE1AK144_ReleaseNotes.txt.(C:\NXP\MC_DevKits\MCSPTE1AK144\MCSPTE1AK144_ReleaseNotes.txt)

The Development Kit application was built and tested using the following IDE and SDK:
=====================================================================================
- S32 Design Studio (S32DS) for ARM 2.2
- S32 Software Development Kit (SDK) for S32K1xx 3.0.2
- FreeMASTER 3.0.3

It is recommended that you follow the tips in Getting Started with the S32K144 BLDC/PMSM Development Kit. (The video in that link also mentioned the need to install S32DS v2.2)


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,225 Views
zhouqichen
Contributor I
Hello, the following documents are currently reported missing
Description Resource Path Location Type
fatal error: gflib.h: No such file or directory actuate_s32k.h /MCSPTE1AK144_PMSM_FOC_1Sh/Sources line 19 C/C++ Problem
"gflib.h" "gmclib.h" "gdflib.h" None of them
0 Kudos
Reply

2,193 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please modify the path of AMMCLIB on your computer

Includes AMMCLIB.jpgLibraries AMMCLIB.jpg

0 Kudos
Reply