MCAL expects source code for code generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCAL expects source code for code generation

Jump to solution
158 Views
kumamon
Contributor II

Hello NXP Support,

MCAL Version: SW32K3_S32M27x_RTD_4.4_4.0.0_P24

When I rename the following .h file to .hh, the ADC generation will fail.

Why is generated source code needed during code generation?

I asked because there is no local source policy in my working place, I can only put non-source code configuration like ARXML in local PC.

kumamon_0-1793356873962.png

 

BR/Kumamon

 

0 Kudos
Reply
1 Solution
135 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @kumamon 

The configuration generation is not necessarily based only on the ARXML. During the generation process, the MCAL configuration tool also require files provided as part of the installed RTD/MCAL package, including header files containing definitions or information required by the generator.

Therefore, if one of the expected .h files is renamed to .hh, the generator may no longer be able to locate or process that dependency, which can cause the code generation to fail.

 

BR, VaneB

View solution in original post

0 Kudos
Reply
2 Replies
135 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @kumamon 

The configuration generation is not necessarily based only on the ARXML. During the generation process, the MCAL configuration tool also require files provided as part of the installed RTD/MCAL package, including header files containing definitions or information required by the generator.

Therefore, if one of the expected .h files is renamed to .hh, the generator may no longer be able to locate or process that dependency, which can cause the code generation to fail.

 

BR, VaneB

0 Kudos
Reply
101 Views
kumamon
Contributor II

Hello @VaneB ,

 

Thanks for your answer.

It is clear now.

 

BR/Kumamon

0 Kudos
Reply