MCAL License Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCAL License Error

2,556件の閲覧回数
lb28
Contributor II

I am trying to configure the MCAL for the NXP S32K14W-Q064 board; EB Tresos is used as the MCAL configuration tool. I’ve downloaded the evaluation version of AUTOSAR 4.2 (S32K1XX_MCAL4_2_RTM_1_0_5)  from NXP. However, once loaded onto the EB Tresos software, the modules yield a “No License for module” error (attached). Any thoughts?

lb28_0-1658421663994.png

 

0 件の賞賛
返信
3 返答(返信)

2,393件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi lb28,

Did you install the license of S32K1XX_MCAL4_2_RTM_1_0_5 correctly?

And Did you install the EB Tresos version correctly with the S32K1XX_MCAL4_2_RTM_1_0_5 package (noted in the release note)?

If the installations are corrected, Could you try to re-install the S32K1XX_MCAL4_2_RTM_1_0_5?

Best regards,

Dan

 

0 件の賞賛
返信

2,405件の閲覧回数
jack_jin
Contributor I

I was in the same situation

0 件の賞賛
返信

2,161件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hello @jack_jin,

Did you download and install the latest license of the S32K1XX_MCAL4_2_RTM_1_0_5 package correctly?

Best regards,

Dan

0 件の賞賛
返信