MCAL GPIO Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCAL GPIO Interrupt

跳至解决方案
3,298 次查看
talha_uyar
Contributor III

Is it possible to configure an interrupt pin through MCAL drivers? If so, how should I configure the EB tresos, and what functions should I use?

I have looked at the s32k148 interrupt example but it uses the function PINS_DRV_Init to configure the interrupt pin as PORT_INT_RISING_EDGE, which is not included in the MCAL.

Thanks in advance,

M. Talha Uyar

标签 (1)
0 项奖励
回复
1 解答
3,229 次查看
hungnguyenphi
NXP Employee
NXP Employee

Dear Muhammet Uyar ,

Please use ICU and PORT module to configure an interrupt pin through MCAL drivers.

Best regards,

Hung.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,230 次查看
hungnguyenphi
NXP Employee
NXP Employee

Dear Muhammet Uyar ,

Please use ICU and PORT module to configure an interrupt pin through MCAL drivers.

Best regards,

Hung.

0 项奖励
回复
3,229 次查看
talha_uyar
Contributor III

Thanks a lot for the help.

0 项奖励
回复