MCAL GPIO Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,285件の閲覧回数
talha_uyar
Contributor III

Is it possible to configure an interrupt pin through MCAL drivers? If so, how should I configure the EB tresos, and what functions should I use?

I have looked at the s32k148 interrupt example but it uses the function PINS_DRV_Init to configure the interrupt pin as PORT_INT_RISING_EDGE, which is not included in the MCAL.

Thanks in advance,

M. Talha Uyar

ラベル(1)
0 件の賞賛
返信
1 解決策
3,216件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Dear Muhammet Uyar ,

Please use ICU and PORT module to configure an interrupt pin through MCAL drivers.

Best regards,

Hung.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,217件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Dear Muhammet Uyar ,

Please use ICU and PORT module to configure an interrupt pin through MCAL drivers.

Best regards,

Hung.

0 件の賞賛
返信
3,216件の閲覧回数
talha_uyar
Contributor III

Thanks a lot for the help.

0 件の賞賛
返信