MC33774ASP1AE : Open-Load Detection for Cell-Terminal Connectivity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC33774ASP1AE : Open-Load Detection for Cell-Terminal Connectivity

跳至解决方案
2,337 次查看
varunbharti
Contributor III

Hello, 

In the MC33774A datasheet (Rev. 2.0, DS743220), section 7.7.1 regarding Cell-terminal pulldown resistors for diagnostic open-load detection of CTx pins mentions the following:

  • A pulldown resistor can be activated between two adjacent cell terminal pins.
  • PRMM_APP_CTRL.VCOLNUM selects which switch is closed, and only one switch can be closed at a time.

Based on this, does it imply that Open-Load Detection for cell-terminal connectivity can only be performed for one cell at a time?

I would greatly appreciate clarification on this functionality.

 

MC33774 

0 项奖励
回复
1 解答
2,302 次查看
RafaR
NXP Employee
NXP Employee

Hi varunbharti

Yes, that is recommended to prevent false measurements by adjacent cells

If you need more information, in the below link you can find in secure files an application note that talks about the open load of this device

https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/18-channel...

RafaR_1-1733945271861.png

 

 

Have a great day and best of luck.

在原帖中查看解决方案

3 回复数
2,303 次查看
RafaR
NXP Employee
NXP Employee

Hi varunbharti

Yes, that is recommended to prevent false measurements by adjacent cells

If you need more information, in the below link you can find in secure files an application note that talks about the open load of this device

https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/18-channel...

RafaR_1-1733945271861.png

 

 

Have a great day and best of luck.

2,188 次查看
varunbharti
Contributor III

Hi,

Thank you for being so supportive. Following your recommendation, I referred to the document you suggested and tested the open-wire diagnostics.

However, I encountered an issue during testing. I opened the wires for 4 cells: C0, C2, C12, and C17.

  • For C0 and C17, I am getting open-load voltages within the expected range.
  • For C2 and C12, I am observing higher-than-expected values.
  • Interestingly, for C2 and C12, the consecutive cells (C3 and C13) are showing the expected values.

Additionally, if I introduce a 100 ms delay between consecutive enabling commands:

  • All cells show results within the expected range.
  • Consecutive cells also show expected values, even if their wires are intact.

Could you please assist in understanding and resolving this issue?

0 项奖励
回复
2,285 次查看
varunbharti
Contributor III
Thankyou
0 项奖励
回复