MC33774A – Questions Regarding ALARM_OUT Pin Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33774A – Questions Regarding ALARM_OUT Pin Configuration

Jump to solution
1,594 Views
varunbharti
Contributor III

Hello NXP Community,

I’m currently working with the MC33774A AFE and have several questions related to the ALARM_OUT pin configuration. I would appreciate your guidance on the following points:

  1. Toggle Functionality: How can I configure the ALARM_OUT pin to toggle whenever any of the configured alarms are triggered?

  2. Enablement: Is there a specific bit or register setting required to activate or enable the ALARM_OUT functionality?

  3. Heartbeat Mode Issues: While testing the ALARM_OUT pin in heartbeat mode, I’ve observed inconsistent behavior—sometimes it works, other times it fails. Has anyone experienced similar issues, or have suggestions for a reliable configuration?

  4. Reconfiguration: Can the ALARM_OUT pin be reconfigured dynamically during runtime, or should it be set only once during initialization?

  5. UV Detection Use Case: I aim to use the ALARM_OUT pin for undervoltage (UV) detection, where the pin should go high when UV is detected. How can I reuse the same pin to detect UV events repeatedly without needing to reconfigure the entire analog front end (AFE)?

  6. Multiple Alarm Events: Is it possible to configure the ALARM_OUT pin to respond to multiple alarm conditions multiple times—i.e., without resetting the MCU or the AFE after each event?

Any insights, register materials, or sample configuration steps would be extremely helpful.

Thank you in advance!

0 Kudos
Reply
1 Solution
1,473 Views
ErikaC
NXP TechSupport
NXP TechSupport
  1. Toggle Functionality: How can I configure the ALARM_OUT pin to toggle whenever any of the configured alarms are triggered?configure FEH_ALARM_CFG (configuration of ALARMOUT signal),  FEH_ALARM_OUT_CFGx (event(s) that will activate ALARMOUT),  and the thresholds (for instance PRMM_AIN0_OV_TH_CFG for an overvoltage detection on AIN0). All configuration information are described in the datasheet.The measurements should be of course enabled (periodic).

  2. Enablement: Is there a specific bit or register setting required to activate or enable the ALARM_OUT functionality?See answer above; when a fault occurs, to clear the ALARMOUT signal, it is required to read both registers FEH_ALARM_OUT_REASON0 and FEH_ALARM_OUT_REASON1

  3. Heartbeat Mode Issues: While testing the ALARM_OUT pin in heartbeat mode, I’ve observed inconsistent behavior—sometimes it works, other times it fails. Has anyone experienced similar issues, or have suggestions for a reliable configuration?what means inconsistent behavior ? when the ALARMOUT hearbeat is activated and no fault occuring then the ALARMOUT toggles permanently at the expected period. No issue reported

  4. Reconfiguration: Can the ALARM_OUT pin be reconfigured dynamically during runtime, or should it be set only once during initialization?yes

  5. UV Detection Use Case: I aim to use the ALARM_OUT pin for undervoltage (UV) detection, where the pin should go high when UV is detected. How can I reuse the same pin to detect UV events repeatedly without needing to reconfigure the entire analog front end (AFE)? you have to clear the ALARMOUT fault reason. You can change the source selection if needed by configuring FEH_ALARM_OUT_CFG0 and CFG1. Don't need to reconfigure the entire analog frontend

  6. Multiple Alarm Events: Is it possible to configure the ALARM_OUT pin to respond to multiple alarm conditions multiple times—i.e., without resetting the MCU or the AFE after each event? yes, see answers above

View solution in original post

0 Kudos
Reply
3 Replies
1,474 Views
ErikaC
NXP TechSupport
NXP TechSupport
  1. Toggle Functionality: How can I configure the ALARM_OUT pin to toggle whenever any of the configured alarms are triggered?configure FEH_ALARM_CFG (configuration of ALARMOUT signal),  FEH_ALARM_OUT_CFGx (event(s) that will activate ALARMOUT),  and the thresholds (for instance PRMM_AIN0_OV_TH_CFG for an overvoltage detection on AIN0). All configuration information are described in the datasheet.The measurements should be of course enabled (periodic).

  2. Enablement: Is there a specific bit or register setting required to activate or enable the ALARM_OUT functionality?See answer above; when a fault occurs, to clear the ALARMOUT signal, it is required to read both registers FEH_ALARM_OUT_REASON0 and FEH_ALARM_OUT_REASON1

  3. Heartbeat Mode Issues: While testing the ALARM_OUT pin in heartbeat mode, I’ve observed inconsistent behavior—sometimes it works, other times it fails. Has anyone experienced similar issues, or have suggestions for a reliable configuration?what means inconsistent behavior ? when the ALARMOUT hearbeat is activated and no fault occuring then the ALARMOUT toggles permanently at the expected period. No issue reported

  4. Reconfiguration: Can the ALARM_OUT pin be reconfigured dynamically during runtime, or should it be set only once during initialization?yes

  5. UV Detection Use Case: I aim to use the ALARM_OUT pin for undervoltage (UV) detection, where the pin should go high when UV is detected. How can I reuse the same pin to detect UV events repeatedly without needing to reconfigure the entire analog front end (AFE)? you have to clear the ALARMOUT fault reason. You can change the source selection if needed by configuring FEH_ALARM_OUT_CFG0 and CFG1. Don't need to reconfigure the entire analog frontend

  6. Multiple Alarm Events: Is it possible to configure the ALARM_OUT pin to respond to multiple alarm conditions multiple times—i.e., without resetting the MCU or the AFE after each event? yes, see answers above

0 Kudos
Reply
1,459 Views
varunbharti
Contributor III
Thankyou
0 Kudos
Reply
1,507 Views
RafaR
NXP Employee
NXP Employee

Please refer to: MC33774A : Question Regarding Alarm and Wakeup Pin Configuration

 

Have a great day and best of luck.

0 Kudos
Reply