Linker file configuration(.ICF) to allow code execution from RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linker file configuration(.ICF) to allow code execution from RAM

4,711件の閲覧回数
ganeshvaka2
Contributor II

Hi,

I am using S32K142 in my design. I am implementing the bootloader using CAN communication. I could get CAN communication up and running. I would like to use the same flash bank for bootloader and application code. I want to copy the code responsible for erasing and flashing the memory to RAM so that I can erase the required sectors on the flash and program the application. 

MCU:S32K142
COMPLIER:IAR

Is there any user guide available for linker configuration (.icf) such that it creates the symbols for required sections of code and it allows to me to copy the code?? 

Note: If you have example linker configuration (.icf) file please share to us 

 Many thanks in advance.

 

Best regards,

Ganesh Babu Vaka

0 件の賞賛
返信
1 返信

4,692件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this is a question rather for IAR, we do not support IAR directly.

But maybe this thread could be helpful:

https://community.nxp.com/t5/Kinetis-Microcontrollers/running-application-in-RAM-with-IAR/m-p/723855

Regards,

Lukas

0 件の賞賛
返信