Lin_Slave_S32K118_Example_DS compile error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lin_Slave_S32K118_Example_DS compile error

1,569 Views
LJX
Contributor I

hi,

I installed S32DS V3.6.2 250529 (Update 2),  SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503_DesignStudio_updatesite.zip and SW32K1_S32M24X_LIN_STACK_2.0.0_D2503_DesignStudio_updatesite.zip.

Then i import Lin_Slave_S32K118_Example_DS, we can see some head files are missing, detail please see the attachment "compiler error.txt".

I tried to search these files in "C:\NXP\S32DS.3.6.2", and added in compile path:

LJX_0-1758943732075.png

but still will report mcu.h -> Mcu_Cfg.h compiler "[!" error:

LJX_2-1758943975919.png

 

Q1: Please help to check is environment problem?

Q2: I try to set LIN stack configuration in S32DS, then port the LIN code to my keil compile environment, can you give some advise?

 

Regards,

 

0 Kudos
Reply
3 Replies

1,516 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@LJX

Have you try to click Update code before compile project?

Senlent_0-1759114685727.png

 

0 Kudos
Reply

1,504 Views
LJX
Contributor I

I try to update the source code, then i will get error:

LJX_1-1759131347768.png

LIN Stack document show support S32DS V3.6, but now I use S32DS V3.6.2, so this is S32DS version problem?

LJX_2-1759131373868.png

 

 

0 Kudos
Reply

1,497 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@LJX

Judging from the error in your screenshot, you haven't installed RTD and LIN STACK properly. Please double-check your installation.

For example, you can try opening some of the examples provided with RTD.

0 Kudos
Reply