Lin_43_LPUART_FLEXIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lin_43_LPUART_FLEXIO

2,358件の閲覧回数
James123
Contributor II

For Lin the irq handler is not hitting after the current state is set as breakfield when the sendframe function is called after that the irq need to hit but it is not hitting,
it is not updating to LPUART_LIN_IP_NODE_STATE_SEND_SYNC because irq is not hitting the irq we are using is Lpuart_Lin_Ip_IRQHandler(1U);  why it is not hitting can you provide more information on this ...

0 件の賞賛
返信
2 返答(返信)

1,558件の閲覧回数
aa4
Contributor I

I'm having the same problem, have you solved it?

タグ(1)
0 件の賞賛
返信

2,346件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

what is a device/board and RTD version you are using? Is interrupt properly enabled for LPUART used?
Anyway the RTD demo example works properly, you can refer to it. 
For LIN transceiver is it active and is there LIN master termination installed?

BR, Petr

0 件の賞賛
返信