LPIT with Fast IRC clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPIT with Fast IRC clock

ソリューションへジャンプ
2,720件の閲覧回数
adrianwenger
Contributor III

Hello,

When i use this LPIT Options

the timer will not work correctly...

 

CC++ - S32K_Timersrctimer.png

-- LPIT timer Settings in timer module

 

CC++ - S32K_Timersrcmain.png

-- the main module

 

 

I use the FIRC as MCU clock and want to use it also al peripheral clock for LPIT...

 

But unfortunately wether the LED nor the A11 Port is toggling.

 

 

What is wrong here?

BR,

Adrian

ラベル(1)
0 件の賞賛
返信
1 解決策
2,372件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Please have look at the attached project.

I have done a few changes in your code, it should work.

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,373件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Please have look at the attached project.

I have done a few changes in your code, it should work.

 

Regards,

Daniel

0 件の賞賛
返信
2,372件の閲覧回数
adrianwenger
Contributor III

Hi Daniel,

thanks now it works!

Regards,

Adrian

0 件の賞賛
返信