LPI2C related doubts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPI2C related doubts

Jump to solution
756 Views
vignesh3
Contributor II

See LpI2C has only one transmit data register MDER.

Then how we can use the FIFO "LPI2C_Set_MasterTxFIFOWatermark" ?

can you give me some idea bout LpI2C fifo?

0 Kudos
Reply
1 Solution
726 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, it is like fifo threshold, to determine when fifo flag is set.
Fifo is not memory mapped.
There is just 1 TX and 1 RX fifo.

BR, Petr

View solution in original post

0 Kudos
Reply
3 Replies
732 Views
vignesh3
Contributor II

Hi @PetrS ,

can you tell me about the watermark is it like fifo threshold or what?

These fifo locations are not memory mapped right? so we can not directly access the fifo.

Can I use 2 fifo for RX and 2 for TX? 

If I can, how I need to configure the watermark for these requirement?

0 Kudos
Reply
727 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, it is like fifo threshold, to determine when fifo flag is set.
Fifo is not memory mapped.
There is just 1 TX and 1 RX fifo.

BR, Petr

0 Kudos
Reply
736 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the LPI2C has 4 deep TX/RX FIFO. A MTDR register is used to write CMD+DATA or DATA into TXFIFO.
You should write MTDR when MSR(TDF) is set indicating whether transmit data is requested. This flag is set when the number of words in the transmit FIFO is equal or less than MFCR[TXWATER]. TXWATER is usually set to 3.

BR, Petr

0 Kudos
Reply