LPCMP comparator with third Input Sample Window

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCMP comparator with third Input Sample Window

1,419 Views
emerging
Contributor III

Hi,

I have a LPCMP0 comparator with one input and a threshold reference voltage, but there is one more input feed back given to the comparator as a Window sample. 

Could you please suggest how to configure and implement this third window input in comparator

Thanks and regards 

Tags (1)
0 Kudos
Reply
1 Reply

1,369 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please read Table 340. Functional modes of S32K3XXRM(Rev8) first, and click to see which Windowed mode you want to implement:
Windowed mode (#5A and #5B)
Windowed/Resampled mode (#6)
Windowed/Filtered mode (#7)

Table 340. Functional modes WINDOW_EN.pngTable 340. Functional modes WINDOW_EN.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply