LIN response error for 2 byte to CANOe (timeout response error )

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LIN response error for 2 byte to CANOe (timeout response error )

2,793 次查看
Sourdev
Contributor II

Hello everyone,

I have been trying to send two bytes of response with 3rd byte as a checksum from my microcontroller(S9KEAZN64AMLC) to the CanOe tool. it is showing a Timeout error for only 2 bytes of the response for every consecutive frame ( if send consecutively one is received and one gives an error it continuously), the same code same system, and the same configuration running flawlessly for 4 bytes, and 8 bytes also.

Configuration is Baud rate is configured for 19200

every transmission and reception done in MCU is from ISR. using  Read data register full Interrupt for reception (request )Interrupt  and Transmission data register empty for Transmission (response)

below is a screenshot attached for the CAN tool receiving data.

Sourdev_0-1679305226543.png

below is the attached LIN bus signal from the logic analyzer.

Sourdev_1-1679305627280.png

 

We tried to fix this issue by increasing jitter in LDF, and instead of configuring Transmission data register empty configuring for Transmission complete Interrrupt still same issue .

 

 

0 项奖励
回复
0 回复数