LIN protocol Tx/Rx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LIN protocol Tx/Rx

1,667件の閲覧回数
semiconductor_user
Contributor III

i am working on s32k324 MCU where i'm tring to commnucation with slave Via Lin protocol.and i am using PLIN tool as slave for data transmit and receive but i'm facing issue in receving data in my board. if anybody have example code for transimt and receive both please share me.

タグ(1)
0 件の賞賛
返信
1 返信

1,638件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there are two RTD demos you can refer to, where LPUART is used as LIN Master
- "Lin_Ip_FrameTransfer_S32K344"...  simple application which shows a communication between a Lin Master and a Lin Slave of both Lpuart Ip and Flexio Ip. But it does not show master receive, however can be modified if needed. 
- "Lin_Master_S32K344_Example_DS" ... LINStack example demonstrating the LIN communication between S32K344 Master and other board/tool Slave using unconditional frames.

PetrS_0-1728479537721.png

If looking for baremetal code, maybe below one can be useful;
https://community.nxp.com/t5/S32K/S32K144-LIN-bus/m-p/818963

BR, Petr

0 件の賞賛
返信