LIN Communication error s32k142

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LIN Communication error s32k142

1,031件の閲覧回数
bhushangs101
Contributor I

Hello Team,
1. I am trying to run 3 way valve but , from code i am getting slave not responding error and
at next iteration time getting slave response as shown in LOG file.
2. i have two log files attached ,
A) One from TLIN PRo software when shedule table is run it runs normally without any errors,
B) when i am running from software code (Attached LIN zip ) it gives response some times and some times gives error - slave not responding., receive Frames drop inconsistently.
please verify the LPUART1_IRQ_handler in LIN.c file

Can you please help to feedback on the same.

1.All Components are giving correct response except response from TWVheatcore (0x33) .
2.Above LOG from CVTMS TACO software is written for only TWVheatcore (0x32) and reading response (0x33).
3.From TACO Software and running from TLINPro software delay are same as per given in LDF.
4.Observation : At start 3 way valve is moving from 100% ->127%->100%->0% , itakes 15 second's to complete its init sequence After that it follows command inputs given from user.
5.Is there any special case we need to read for TWVheatcore response(0x33) ? and Delay adjustments?

0 件の賞賛
返信
1 返信

992件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

discussed over individual Case already.

BR, Petr

0 件の賞賛
返信