KeyDerivation Copy parameters issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KeyDerivation Copy parameters issue

跳至解决方案
1,104 次查看
kerti1
Contributor III

Hi @lukaszadrapa ,

 

I used the keyderiveCopyKeyReq struct to get the key for my AES encryption. I am sure that my key catalog is correct. My keyhandle points to the Shared key that i derived using the keyderiveReq and which I stored in the RAM key handle with group index as 3. The targethandle to the new RAM catalog for the AES. After all these still i get the invalid_params. Please help me in finding out the issue

标记 (2)
0 项奖励
回复
1 解答
1,037 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @kerti1 

This is original function from HSE Demo Examples:

lukaszadrapa_0-1748871362133.png

The key point - whole descriptor is erased before next use.  This is not implemented in your code, so there are some leftovers from previous operations. Let's compare parameters in your original version:

lukaszadrapa_1-1748871454198.png

... with version when the descriptor was cleared at the beginning (I did that manually in my debugger):

lukaszadrapa_2-1748871502302.png

As you can see, I got HSE_SRV_RSP_OK when the descriptor is erased before setting of parameters. Obviously HSE could not accept those messed parameters.

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,059 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @kerti1 

Could you share whole project, so I can check it on my side? I can't see a problem in the parameters.

Regards,

Lukas

0 项奖励
回复
1,055 次查看
kerti1
Contributor III

Hi @lukaszadrapa,

 

Thanks for the response. Please find the attached project. Thank you in advance.

0 项奖励
回复
1,038 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @kerti1 

This is original function from HSE Demo Examples:

lukaszadrapa_0-1748871362133.png

The key point - whole descriptor is erased before next use.  This is not implemented in your code, so there are some leftovers from previous operations. Let's compare parameters in your original version:

lukaszadrapa_1-1748871454198.png

... with version when the descriptor was cleared at the beginning (I did that manually in my debugger):

lukaszadrapa_2-1748871502302.png

As you can see, I got HSE_SRV_RSP_OK when the descriptor is erased before setting of parameters. Obviously HSE could not accept those messed parameters.

Regards,

Lukas

0 项奖励
回复
978 次查看
kerti1
Contributor III
Thank you
0 项奖励
回复
1,068 次查看
kerti1
Contributor III

Hi,

 

Could someone please let me know what is the issue. It would be really helpful. 

 

0 项奖励
回复