KITFS85SKTEVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KITFS85SKTEVM

9,605 Views
yavuzklcc
Contributor III

Hello everyone

While trying to program the FS8530 chip on the KITFS85SKTEVM board,I encounter an error,I get the error ABIST2 FAIL.And it gets stuck in INIT_SAFE mode.

What can be done?

Thx. 

0 Kudos
Reply
18 Replies

9,584 Views
yavuzklcc
Contributor III

hata.png

Fault screen

0 Kudos
Reply

9,588 Views
yavuzklcc
Contributor III

When i send FS_OVUVREG_STATUS message (VCOREMON_UV bit is 1) ,under voltage fault is fixed,but abıst2 fault continue.

0 Kudos
Reply

9,553 Views
guoweisun
NXP TechSupport
NXP TechSupport

If fixed the Vcore UV issue,without other issue the ABIST2 will PASS. 

 

0 Kudos
Reply

9,548 Views
yavuzklcc
Contributor III
Thanks for answer.
Yes,but VCore UV issue dont fixed.What could be the source of the problem ?
0 Kudos
Reply

9,491 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can check the Vcore related circuit to verify it again,I attached the schematic for you review.

 

 

0 Kudos
Reply

9,481 Views
yavuzklcc
Contributor III

 At the same time, I apply these steps exactly. But when I send the message to exit DEBUG mode,

1-) all regulators power on and the

2-)all regulators power off and RESET pin blinks 3 times.

This cycle continues.Something seems to be going wrong.

Iam beginner, i will be glad if you help

 

hata3.png

 

0 Kudos
Reply

9,456 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please follow up the app note for operating this SBC step by step.

Better for your test used the programmed chip by NXP you can order this part instead of blank part OTP by yourself.

After familiar with EVB then you can do OTP by yourself.

 

 

0 Kudos
Reply

9,487 Views
yavuzklcc
Contributor III
I checked the VCOREMON pin. It doesn't see any problem . It is connected with BUCK1.
0 Kudos
Reply

9,542 Views
guoweisun
NXP TechSupport
NXP TechSupport

did you test the Vcore in your board? does it match what you setting value?

If Vcore is good,ABIST2 will pass no issue.

 

0 Kudos
Reply

9,525 Views
yavuzklcc
Contributor III
I knows that there is no point where I can measure Vcore directly. When I measure BUCK1 it matches the value i set.
0 Kudos
Reply

9,521 Views
guoweisun
NXP TechSupport
NXP TechSupport

Does any error show in the GUI OV/UV or others iteam after your fixed VCORE?

0 Kudos
Reply

9,519 Views
yavuzklcc
Contributor III

hata1.png

After opening the card I only see the VCORE UV issue. 

0 Kudos
Reply

9,550 Views
guoweisun
NXP TechSupport
NXP TechSupport

If in the OTP just as below picture showed, in the ABIST1,you enable the monitor of  VCORE/VDDIO/VMONX by OTP, in the  ABIST2 can  monitor VCORE/VDDIO/VMON1234 ,any error the SBC will hang. especially for the VMONX the reference voltage is 0.8V.

guoweisun_0-1677029306599.png

 

 

 

0 Kudos
Reply

9,584 Views
yavuzklcc
Contributor III

Yes.SBC stuck in ABIST2 phase.

hata.png

 

0 Kudos
Reply

9,594 Views
guoweisun
NXP TechSupport
NXP TechSupport

Or can you give some picture for your error?

 

0 Kudos
Reply

9,597 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you mean the SBC stuck in ABIST2 phase when start up in your board?

 

 

0 Kudos
Reply

9,581 Views
yavuzklcc
Contributor III
Yes.SBC stuck in ABIST2 phase.When i sent FS_OVUVREG_STATUS (VCOREMON bits is 1),under voltage fault is fixed ,but ABIST2 fault still continue.i will share you picture fault screen.
0 Kudos
Reply

9,570 Views
yavuzklcc
Contributor III
I tried but nothing change.
0 Kudos
Reply