Issues with the support for Express programming of Flash in the RTD for S32K312

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with the support for Express programming of Flash in the RTD for S32K312

Jump to solution
864 Views
Chris-Sun
Contributor II
According to the S32K3x manual, Flash supports the Express program feature.
I have created an S32K312 project, but I couldn't find any interfaces or implementations related to Express programming in the RTD. Could you please clarify if the RTD does not support this feature or if it needs to be implemented manually?
 
 
The version information:
 

S32DS: 3.5

RTD: S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331

Best regards,
Chris

0 Kudos
Reply
1 Solution
829 Views
CongDang
NXP Employee
NXP Employee

Hi Chris, Thanks for your question!

Unfortunately, currently, the RTD does not support this feature (I guess because we don't have any requirement for the feature).

View solution in original post

0 Kudos
Reply
4 Replies
830 Views
CongDang
NXP Employee
NXP Employee

Hi Chris, Thanks for your question!

Unfortunately, currently, the RTD does not support this feature (I guess because we don't have any requirement for the feature).

0 Kudos
Reply
827 Views
Chris-Sun
Contributor II

Hi @CongDang 

Thank you for your response to my post.

According to the manual, S32K3X Flash supports "Express Program" feature.
Can I manually implement it based on the instructions provided in the manual?
 
Best regards,
Chris
0 Kudos
Reply
765 Views
CongDang
NXP Employee
NXP Employee

Yes, I think it's a good solution for this case.

0 Kudos
Reply
755 Views
Chris-Sun
Contributor II

Thank you for your response to my post.

 
Best regards,
Chris
0 Kudos
Reply