Issues with the support for Express programming of Flash in the RTD for S32K312

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issues with the support for Express programming of Flash in the RTD for S32K312

跳至解决方案
766 次查看
Chris-Sun
Contributor II
According to the S32K3x manual, Flash supports the Express program feature.
I have created an S32K312 project, but I couldn't find any interfaces or implementations related to Express programming in the RTD. Could you please clarify if the RTD does not support this feature or if it needs to be implemented manually?
 
 
The version information:
 

S32DS: 3.5

RTD: S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331

Best regards,
Chris

0 项奖励
回复
1 解答
731 次查看
CongDang
NXP Employee
NXP Employee

Hi Chris, Thanks for your question!

Unfortunately, currently, the RTD does not support this feature (I guess because we don't have any requirement for the feature).

在原帖中查看解决方案

0 项奖励
回复
4 回复数
732 次查看
CongDang
NXP Employee
NXP Employee

Hi Chris, Thanks for your question!

Unfortunately, currently, the RTD does not support this feature (I guess because we don't have any requirement for the feature).

0 项奖励
回复
729 次查看
Chris-Sun
Contributor II

Hi @CongDang 

Thank you for your response to my post.

According to the manual, S32K3X Flash supports "Express Program" feature.
Can I manually implement it based on the instructions provided in the manual?
 
Best regards,
Chris
0 项奖励
回复
667 次查看
CongDang
NXP Employee
NXP Employee

Yes, I think it's a good solution for this case.

0 项奖励
回复
657 次查看
Chris-Sun
Contributor II

Thank you for your response to my post.

 
Best regards,
Chris
0 项奖励
回复