Issue in capturing Change Frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue in capturing Change Frequency

967件の閲覧回数
shrikantkoli1995
Contributor I

Hi Team,

I am working with s32k344 series.

Description :

If i set the frequency 1Khz and set the duty 20 %,40% and 60% the ICU get this duty and it will visible into the debug window. But at the runtime if i change the frequency from 1Khz to 2khz and then again i will set the duty for the same frequency like 20 %,40% and 60% that time input capture unit capture the wrong duty cycle.

 

Is their any limitation for input capture unit?

Regards,

Shrikant K

 

0 件の賞賛
返信
1 返信

950件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there should not be limitation, but check if overflows could not happen on selected counter base. If yes try to modify channel prescaler.

BR, Petr

0 件の賞賛
返信