Issue in capturing Change Frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue in capturing Change Frequency

1,014 Views
shrikantkoli1995
Contributor I

Hi Team,

I am working with s32k344 series.

Description :

If i set the frequency 1Khz and set the duty 20 %,40% and 60% the ICU get this duty and it will visible into the debug window. But at the runtime if i change the frequency from 1Khz to 2khz and then again i will set the duty for the same frequency like 20 %,40% and 60% that time input capture unit capture the wrong duty cycle.

 

Is their any limitation for input capture unit?

Regards,

Shrikant K

 

0 Kudos
Reply
1 Reply

997 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there should not be limitation, but check if overflows could not happen on selected counter base. If yes try to modify channel prescaler.

BR, Petr

0 Kudos
Reply