Issue Opening .mex File for Unified Bootloader RTD Migration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue Opening .mex File for Unified Bootloader RTD Migration

630 Views
Aravind_Togaralli
Contributor II

Hi,

Currently, I am working on the Unified Bootloader with RTD version 2.0.0, and we need to migrate it to RTD version 7.0.0.

To proceed with the migration, we need to understand which peripherals are enabled and how they are configured. Normally, we can verify these details by opening the .mex file. However, in our case, the .mex file is not opening.

My current setup is:

S32 Design Studio for S32 Platform
Version: 3.6.5
Build ID: 251127

Could you please let us know how this issue can be resolved?

Is there Any other suggested Method for migration?

Is it possible to open the project by using a lower IDE version or any other compatible setup?

Reference: Unified Bootloader download from the below thread:
Unified Bootloader Demo Thread

Aravind_Togaralli_1-1779369909997.png

 

 

Thanks.

0 Kudos
Reply
1 Reply

600 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Aravind_Togaralli 

The Unified Bootloader Demo for S32K3 devices was developed and tested using RTD version 2.0.0 and S32DS 3.4. To ensure compatibility, please use these software versions when working with this project.

 

BR, VaneB

0 Kudos
Reply