Is OpenSDA supported for S32K2 evaluation board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is OpenSDA supported for S32K2 evaluation board?

1,329 Views
veeresh_ambe
Contributor III

Hi all,

I wanted to know if OpenSDA is supported on the S32K2TV evaluation board? The schematic shows that there is a openSDA connection available to the controller but the S32 IDE does not detect the connection(pls see attached screenshot). How do you usually connect to the board? Is it through a Multilink probe or Lauterbach probe?

S32K2_openSDA.png

0 Kudos
Reply
1 Reply

1,315 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

OpenSDA should be able to connect, PEMicro and multilink should also work.

Eventually you can use S32 Debug probe which is most commonly used with K2 and K3 micros.

best regards,

Peter

0 Kudos
Reply