Hi @rohans002 ,
I have tested the data transmission and reception of this example and observed consistent behavior, the master receives the response from the slave device and the LED turns green, see the image below:

Please make sure the board is powered by 12V and follow the steps on how to run the example in C:\NXP\S32DS.3.4\S32DS\software\S32SDK_S32K1XX_RTM_4.0.3\doc\html_S32K144\lin_master_baremetal_s32k144_group.html.
Note: These examples are intended to be used with 2 EVKs (S32K144), so you can also refer to the document for the slave device in C:\NXP\S32DS.3.4\S32DS\software\S32SDK_S32K1XX_RTM_4.0.3\doc\html_S32K144\lin_slave_baremetal_s32k144_group.html.

BR,
IsaulO.