Interrupt Callback for DMA in MPC(Multiple Parallel Conversion) not getting generated (DMA trig).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt Callback for DMA in MPC(Multiple Parallel Conversion) not getting generated (DMA trig).

Jump to solution
1,192 Views
AkhileshBelore
Contributor I

Hello,
(For S32K39-37 (S32K396))
The below mentioned signals are connected to the respective ADCs as per the below table: 

SignalsADCCL attributesFIFO
SIN_PADC3_P2List StartFIFO 1
COS_PADC5_P0 
SIN_Inv_PADC3_P1 
COS_Inv_PADC5_P1Last channel

 

Here, BCTU shall be triggered and data from the above ADCs shall be stored in FIFO1 which shall be further be accessed through DMA.

Currently through debugging it can be observed that BCTU is getting triggered, FIFO is getting updated, source and destination for DMA are as expected, interrupt is also enabled but interrupt callback mentioned in DMA is not getting trigger.

Please check the below doc.("Configurations.docx") for all the respective configurations.

0 Kudos
Reply
1 Solution
1,150 Views
AkhileshBelore
Contributor I

SOLVED.
Had missed updating "Dma Mux Source"

AkhileshBelore_0-1730961439860.png

 

View solution in original post

0 Kudos
Reply
2 Replies
1,151 Views
AkhileshBelore
Contributor I

SOLVED.
Had missed updating "Dma Mux Source"

AkhileshBelore_0-1730961439860.png

 

0 Kudos
Reply
1,166 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @AkhileshBelore,

Did you enable the DMA interrupt in the Interrupt driver?

 

0 Kudos
Reply