Integration of S32K144EVB with Motor GD3000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Integration of S32K144EVB with Motor GD3000

931件の閲覧回数
rajangingee
Contributor I

hi Team, 

i recently bought s32k144EVB, Linix(45ZWN424-40) BLDC motor & GD3000 Motor Devkit separately... i am following the instructions mentioned in the example model to adjust the jumpers & also the resistors below 

R168/R166 are placed & R167/R165 are removed... 

can you please elaborate me like what needs to be done here ? 

Also please let me know is there any other steps that i need to consider 

0 件の賞賛
返信
3 返答(返信)

907件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Thank you so much for your interest in our products and for using our community.

You can follow the Getting Started with the S32K144 BLDC/PMSM Development Kit, which come in the Documentation section from MCSPTE1AK144 page.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信

853件の閲覧回数
rajangingee
Contributor I

hi, 

i was able to run the motor using devkit GD & S32k144 with linik motor from the PMSM open loop model available in s32MBD toolkit

while i reduced my speed to zero & then starting again, i found the motor stall & after that my motor doesnt run (this was done using MATHWORKS example (FOC for PMSM with hall sensor using MCSPTEAK144) - where the host model sends speed reference via serial communication)

observed that Motor DEVKIT gets heaten up & im also getting continuity between all capacitors & Q2 mosfet - all terminals are shorted i think. the board gets heated & my D2 LED is blinking 

im getting only 0.5 to 1.2V between the terminals of D2

note: the trimpot in DEVKIT is rotated CCW to its max position  

please advice me to proceed further 

0 件の賞賛
返信

819件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

For questions related to MBDT we have a specific forum, where experts on the subject can help you. I am going to ask you please to direct the related questions in the following community:

Model-Based Design Toolbox (MBDT)

I appreciate your understanding.

Have a nice day!

0 件の賞賛
返信