Initialize NfcLib_Init()

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Initialize NfcLib_Init()

1,865 Views
zhouwe35
Contributor I

When executing the function phNfcLib_Init(), it will return PH_STATUS_INPROCESS a couple of times at first, and when proceeding further, it will return PH_ERR_ABORTED The configuration of the lpTMR module is as follows

zhouwe35_0-1729059305368.png

 

0 Kudos
Reply
3 Replies

1,838 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @zhouwe35

Hope you are doing well.

Could you please provide more details on your setup? What is the device you are using?

Also, are you using the NFC Reader Library? If so, what is the version you are using?

Regards,
Eduardo.

0 Kudos
Reply

1,822 Views
zhouwe35
Contributor I

Hi, Eduardo

Thank you for your reply, I use window for my device, now I am porting NFC Reader Library on other MCUs, the version is aNfcRdLib_SDK_Evaluation_v2.32, the chip I choose is 3321, I have already configured the required spi communication pins, Reset and interrupt pins in the MCU, but when I execute Figure 1, phNfcLib_Init(), I can see that it is a good choice for me. can I trouble you to help see if there is any problem, or the pin configuration of the side to be What rules should I follow?

 

图1

 

图2

 

图3

 

图4

 

 

 

 

 

0 Kudos
Reply

1,813 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I just sent you a private Community message.

Have a nice day!

Regards,
Eduardo.

0 Kudos
Reply