Initialize NfcLib_Init()

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Initialize NfcLib_Init()

1,929件の閲覧回数
zhouwe35
Contributor I

When executing the function phNfcLib_Init(), it will return PH_STATUS_INPROCESS a couple of times at first, and when proceeding further, it will return PH_ERR_ABORTED The configuration of the lpTMR module is as follows

zhouwe35_0-1729059305368.png

 

0 件の賞賛
返信
3 返答(返信)

1,902件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @zhouwe35

Hope you are doing well.

Could you please provide more details on your setup? What is the device you are using?

Also, are you using the NFC Reader Library? If so, what is the version you are using?

Regards,
Eduardo.

0 件の賞賛
返信

1,886件の閲覧回数
zhouwe35
Contributor I

Hi, Eduardo

Thank you for your reply, I use window for my device, now I am porting NFC Reader Library on other MCUs, the version is aNfcRdLib_SDK_Evaluation_v2.32, the chip I choose is 3321, I have already configured the required spi communication pins, Reset and interrupt pins in the MCU, but when I execute Figure 1, phNfcLib_Init(), I can see that it is a good choice for me. can I trouble you to help see if there is any problem, or the pin configuration of the side to be What rules should I follow?

 

图1

 

图2

 

图3

 

图4

 

 

 

 

 

0 件の賞賛
返信

1,877件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I just sent you a private Community message.

Have a nice day!

Regards,
Eduardo.

0 件の賞賛
返信