Incompatible IDE version issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Incompatible IDE version issue

1,125 Views
worter
Contributor I

Our company is using version 3.5 of the IDE along with its corresponding software support package, RTD. I downloaded version 3.6 of the IDE, but it cannot import our software package or RTD. The official website provides a download link for the 3.5 IDE, but this version requires a license, and there is no longer a license acquisition link available for version 3.5 on the website. Is there any way to resolve this issue?

0 Kudos
Reply
3 Replies

1,104 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

If you insist on using the same software as your colleagues, then try downloading S32DS v3.5 and it's Update from S32 Design Studio - Releases & Updates.

However, according to the information in the "S32 Design Studio 3.6.0 Release Announcement", it should be compatible with the S32K3 RTD you mentioned:
RTD and Runtime Software releases made on top of S32Design Studio 3.5.x are backward compatible with S32Design Studio 3.6.0 using smart compatibility mechanism

Please refer to the instructions in the video(How To Download, Install and Configure the RTD 5.0.0 with S32 Design Studio 3.6.0) to download and install the specific version of S32K3 RTD that you need. 

And don't forget to install NXP GCC for Arm Embedded Processors v10.2 build 1728

BMS_SWInstallationGuide_NXP_V8_final S32DSv3.6.6 GCC v10.2.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

0 Kudos
Reply

902 Views
worter
Contributor I
Our RTD version here is 2.0.0. I tried importing the 3.6 version of the IDE but it failed. Currently, only the 3.5 download package is available on the website, and there is no license key. At that time, the 3.5 IDE would use the license key during the download process, and it got stuck at this issue.
0 Kudos
Reply

864 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

请问你是否在S32 Design Studio - Releases & Updates里点击Flexera下载S32DSv3.5? 

Download S32DS v3.5.png

如果邮箱没有收到Activation Code(还请检查是否被当作垃圾邮件了),那么请在License Keys选项里找到Activation Code。

Activation Code License Keys S32 Design Studio for S32 Platform v.3.5.png

0 Kudos
Reply