Inaccurate sampling in S32K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inaccurate sampling in S32K

857 Views
Hailong_Zeng
Contributor I

企业微信截图_17356334435198.png

The multimeter measures FUEL_SENSOR_1_CAPACITAL1 1.3 mV, but the actual value printed by the MCU serial port is 7mV.Is it the sampling network that's incorrect?

0 Kudos
Reply
1 Reply

827 Views
PavelL
NXP Employee
NXP Employee

Hello @Hailong_Zeng ,

I apologize for late response caused by Xmas vacations.

At first look, your C4116 and C4117 have low capacitance. Please refer to AN4373, Cookbook for SAR ADC Measurements - Application note (nxp.com) . E.g. for S32K3, necessary information (CS, CP1, CP2, RSW, RAD, ...) to calculate values of external components can be found in chapter 10.1 of S32K3 data sheet.

While you are sensing mV, I also recommend to have separate ground path for your signal from source to MCU. The ground path shall be separated in a way that no other current flows through this path.

Best regards,

Pavel

0 Kudos
Reply