ISO 16825

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISO 16825

1,553件の閲覧回数
powm
Contributor I

Is the HW CAN module for FS32K118BRT0VLFR conform with ISO 16845?

Question from customer.

0 件の賞賛
返信
1 返信

1,541件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

The CAN conformance test report for the s32k1xx devices can be share only via a support ticket.

However, we can found there the information below.

CAN Conformance Test:
ISO/DIS16845-1:2016 Road vehicles - Controller area network (CAN)

Conformance Test Results:

(The Test Results refer to the delivered device and the applicable test cases.)

ISO CAN conformance tests:
Classic CAN: PASS
Classic CAN + FD: enabled PASS
FD CAN + CAN FD: enabled PASS

If you need the whole report, please, create a support ticket.

Thank you.

Best regards,

Diana

0 件の賞賛
返信