ICU IPWM Capture Cycle Loss

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ICU IPWM Capture Cycle Loss

Jump to solution
2,342 Views
Du_0224
Contributor III

Hello NXP engineers.

Test environment:

S32K314 + RTD2.0.2

* Autosar Version : 4.4.0
* Autosar Revision : ASR_REL_4_4_REV_0000
* Autosar Conf.Variant :
* SW Version : 2.0.2
* Build Version : S32K3_RTD_2_0_2_D2211_ASR_REL_4_4_REV_0000_20221129

 

I'm testing with an IPWM acquisition lost cycle problem.

IPWM clock 1M
A jump problem was found during testing of the 3K 50% duty cycle.
Troubleshooting with an oscilloscope, the waveforms from the hardware input to the MCU are correct. There is no cycle loss problem

And the value after the jump is basically around 1.5K, 75% duty cycle.

Based on the phenomenon it is suspected that the IPWM acquisition is missing a cycle?

Du_0224_0-1704191071964.png

Du_0224_2-1704191146143.png

Du_0224_3-1704191152996.png

 

1M clock, counting: 3KHz, 50% duty cycle. The count should be: period value ≈ 333, A-B ≈ 167.

According to the phenomenon, the pulse width is correct, but the duty cycle is calculated incorrectly because the period value is not correct.
The debug adds variables to save the time of arrival of each pulse edge:

Du_0224_4-1704191195511.png

The test found that the value latched into register B is just not right:

Du_0224_5-1704191235621.png

 

 

 

Tags (1)
0 Kudos
Reply
1 Solution
2,304 Views
Du_0224
Contributor III

Problem solved, this issue is closed

View solution in original post

0 Kudos
Reply
2 Replies
2,322 Views
Du_0224
Contributor III

I performed a further test by doing a register read at the interrupt general entry, but the phenomenon is the same.

Du_0224_2-1704253284189.png

 

Du_0224_1-1704253256812.png

 

0 Kudos
Reply
2,305 Views
Du_0224
Contributor III

Problem solved, this issue is closed

0 Kudos
Reply