ICU IPWM Capture Cycle Loss

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ICU IPWM Capture Cycle Loss

跳至解决方案
2,344 次查看
Du_0224
Contributor III

Hello NXP engineers.

Test environment:

S32K314 + RTD2.0.2

* Autosar Version : 4.4.0
* Autosar Revision : ASR_REL_4_4_REV_0000
* Autosar Conf.Variant :
* SW Version : 2.0.2
* Build Version : S32K3_RTD_2_0_2_D2211_ASR_REL_4_4_REV_0000_20221129

 

I'm testing with an IPWM acquisition lost cycle problem.

IPWM clock 1M
A jump problem was found during testing of the 3K 50% duty cycle.
Troubleshooting with an oscilloscope, the waveforms from the hardware input to the MCU are correct. There is no cycle loss problem

And the value after the jump is basically around 1.5K, 75% duty cycle.

Based on the phenomenon it is suspected that the IPWM acquisition is missing a cycle?

Du_0224_0-1704191071964.png

Du_0224_2-1704191146143.png

Du_0224_3-1704191152996.png

 

1M clock, counting: 3KHz, 50% duty cycle. The count should be: period value ≈ 333, A-B ≈ 167.

According to the phenomenon, the pulse width is correct, but the duty cycle is calculated incorrectly because the period value is not correct.
The debug adds variables to save the time of arrival of each pulse edge:

Du_0224_4-1704191195511.png

The test found that the value latched into register B is just not right:

Du_0224_5-1704191235621.png

 

 

 

标记 (1)
0 项奖励
回复
1 解答
2,306 次查看
Du_0224
Contributor III

Problem solved, this issue is closed

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,324 次查看
Du_0224
Contributor III

I performed a further test by doing a register read at the interrupt general entry, but the phenomenon is the same.

Du_0224_2-1704253284189.png

 

Du_0224_1-1704253256812.png

 

0 项奖励
回复
2,307 次查看
Du_0224
Contributor III

Problem solved, this issue is closed

0 项奖励
回复