Hi,
I'm currently trying to test the transfer between the K3x4EVB-T172 board with an EEPROM with LPI2C1.
I'm using the LPI2C Transfer k344 example as the base.
When trying to measure the SCL with an oscilloscope, the clock signal doesn't show an 8 bit signal.
When using the Lpi2c_Ip_MasterSendData() or Lpi2c_Ip_MasterReceiveData(), there should be 8 bits shown on the scope, but it just show one quick low high signal.
Is there a certain setting missing or am I misunderstanding how to use s32ds?
I'm trying to code by following the datasheet for EEPROM; however, in order to verify if the everything is working properly, I'm trying to test with the scope.
Thank You.
已解决! 转到解答。
Hi
Please refer to the discussion in S32K312 - How can I set I2C baud rate? Note LPI2C Timing Parameter Restrictions
Also, are there any pull-up resistors connected to the I2C pins?
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
Please refer to the discussion in S32K312 - How can I set I2C baud rate? Note LPI2C Timing Parameter Restrictions
Also, are there any pull-up resistors connected to the I2C pins?
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------