How to use ProcessorExpert set system clock to 80MHz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use ProcessorExpert set system clock to 80MHz?

1,651 Views
w_lingjun
Contributor III

Hi All,

I'm using S32K142 to develope, my S32DS version is "S32 Design Studio for ARM Version 2018.R1". And there is a  function named ProcessorExpert, it can config settings by GUI.

In the reference manual, normal RUN mode, the core and system clock can be set to 80MHz

But in the PE, it just can be set to 48MHz. So how to use PE set system clock to 80MHz?

1 Reply

1,571 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

Please refer to the following community post. 

Have a great day,

Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------