Hi
My S32K116EVB2Q048 is the SCH-47484 REV A version. J107 connects 1-2 to use P5V_SBC for power supply. Power the board with external 12V at J16 without debugger. At this time, I am able to see the waveform of SPI0_PCS0 on PTB0.
I measured the PTB0 signal through J3.2, and the R754 on the bottom of the board is soldered.
The tested project only changed the PCS pin of lpspi_dma_master_s32k116_SDK403 from PTB5 to PTB0.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------