How to specify PEmicro to execute pegdbserver_console.exe -startserver -device=NXP_S32K146F1M0M11

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to specify PEmicro to execute pegdbserver_console.exe -startserver -device=NXP_S32K146F1M0M11

2,480 次查看
Jackey_cj
Contributor I

I want to do automated testing, with one computer connected to two PEmicro devices. The ports for the two devices are different, they are PE5748112 and PE5750306 respectively, and they are connected to S32K146 and S32K148 boards. How do I specify a particular PEmicro to execute the programming command?I hope this job can be done through the command line.

0 项奖励
回复
2 回复数

2,396 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

you can specify interface and port when you start pegdbserver_console for example like this: 

pegdbserver_console.exe -startserver -device=NXP_S32K3xx_S32K312 -interface=USBMULTILINK -port=PEMB7D193

 

More commands you can find with pegdbserver_console.exe --help  command. 

0 项奖励
回复

2,231 次查看
Jackey_cj
Contributor I

Hi,

I want to specify a PE to start a corresponding service when using the command line, but my specification doesn't seem to take effect; it keeps using the default value. As shown in the image, my computer is connected to two PEs: PE5748112 and PE5750673. However, when I try to specify PE5750673 using "-port" or "-PORT," it still defaults to using PE5748112, which is the HW Auto-Selected case. How can I resolve this issue?

0 项奖励
回复