How to set attributes of CSEc key

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set attributes of CSEc key

2,309 Views
wang_q4
Contributor I

Dear All,

I want to set attributes(BOOT_PROT、DEBUG_PROT、KEY_USAGE、WILDCARD、VERIFY_ONLY) of CSEc keys,but i don't know where to set it?

0 Kudos
Reply
4 Replies

2,302 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @wang_q4,

Please refer to AN5401 Getting Started with CSEc Security Module.

danielmartynek_0-1626254119044.png

the below code is from csec_utils.c (csec_keyconfig_s32k1xx SDK example)

danielmartynek_1-1626254354015.png

You could add the attributes before it is encrypted.

uint8_t FID = 0x00;  // or set FID = WRITE_PROTECTION | BOOT_ PROTECTION | DEBUGGER_PROTECTION | KEY_USAGE | WILDCARD
/* Calculate flag value */
m2Plain[3] |= (FID & 0xF0) >> 4;
m2Plain[4] |= (FID & 0x0F) << 4;

 

Regards,

Daniel

 

0 Kudos
Reply

1,829 Views
ZEROOO
Contributor IV

Hi Daniel

    Referring to this figure, I would like to ask if if SFE=0x00, FID=0b00010 should be set in computeM1M2M3 if the key is to be used for CMAC generation, similarly, if SFE=0x01, if the key is to be used for CMAC generation FID=0x000100, I wonder if there is any problem with this understanding.

    In addition, I set FID=0b00010 in computeM1M2M3, which caused an error when I updated the key. What was strange was that the first key update was normal, but the error occurred in the second update. Could you please explain?The following is the update I made, please point out if there are any mistakes, thank you very much.

ZEROooo_0-1680788582433.png

 

ZEROooo_1-1680788781925.pngZEROooo_2-1680788869379.png

 

0 Kudos
Reply

2,287 Views
wang_q4
Contributor I

I load the key according to the following code,

but I have returned "STATUS_SEC_KEY_WRITE_PROTECTED" when restoring the factory settings

status_t CSEcDrv_ComputeM1M2M3(uint8_t* p_auth_key, csec_key_id_t auth_id, csec_key_id_t key_id, const uint8_t* p_key, uint32_t counter,
uint8_t* p_uid, uint8_t* p_m1, uint8_t* p_m2, uint8_t* p_m3, bool boot_protection)
{
status_t stat;
uint8_t FID = 0x00;
uint8_t i;
uint8_t iv[16] = {0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0};

uint8_t k1[16];
uint8_t k2[16];

uint8_t m2Plain[32];

uint8_t m1m2[48];

/* Derive K1 and K2 from AuthID */
CSEcDrv_KDF(p_auth_key, key_update_enc_c, k1);
CSEcDrv_KDF(p_auth_key, key_update_mac_c, k2);

/* Compute M1 = UID | ID | AuthID */
for (i = 0; i < 15; i++)
{
p_m1[i] = p_uid[i];
}
p_m1[15] = ((key_id & 0xF) << 4) | (auth_id & 0xF);

/* Compute M2 (C = counter, F = 0) */
for(i = 0; i < 16; i++)
{
m2Plain[i] = 0;
m2Plain[16 + i] = p_key[i];
}
m2Plain[0] = (counter & 0xFF00000) >> 20;
m2Plain[1] = (counter & 0xFF000) >> 12;
m2Plain[2] = (counter & 0xFF0) >> 4;
m2Plain[3] |= (FID & 0xF0) >> 4;
m2Plain[4] |= (FID & 0x0F) << 4;

/* Encrypt M2 */
stat = CSEC_DRV_LoadPlainKey(k1);
if (stat != STATUS_SUCCESS)
{
return stat;
}

stat = CSEC_DRV_EncryptCBC(CSEC_RAM_KEY, m2Plain, 32U, iv, p_m2, 1U);
if (stat != STATUS_SUCCESS)
{
return stat;
}

/* Compute M3 as CMAC(key=k2, m1|m2)*/
for (i = 0; i < 16; i++)
{
m1m2[i] = p_m1[i];
}
for(i = 0; i < 32; i++)
{
m1m2[16 + i] = p_m2[i];
}

stat = CSEC_DRV_LoadPlainKey(k2);
if (stat != STATUS_SUCCESS)
{
return stat;
}

stat = CSEC_DRV_GenerateMAC(CSEC_RAM_KEY, m1m2, 384U, p_m3, 1U);
if (stat != STATUS_SUCCESS)
{
return stat;
}

return STATUS_SUCCESS;
}

status_t CSEcDrv_EraseKeys_Sync(void)
{
status_t stat;
uint8_t auth_key[16];
uint8_t challenge[16];
uint8_t auth[16];
uint8_t auth_plain[31];
uint8_t k[16];
uint8_t uid[15];

uint8_t i;

CSEcDrv_GenerateMasterKey(&auth_key[0]);
CSEcDrv_GetUID_Sync(uid);

CSEcDrv_KDF(auth_key, key_debug_key_c, k);

stat = CSEC_DRV_LoadPlainKey(k);
if (stat != STATUS_SUCCESS)
{
return stat;
}

stat = CSEC_DRV_DbgChal(challenge);
if (stat != STATUS_SUCCESS)
{
return stat;
}

for (i = 0; i < 16; i++)
{
auth_plain[i] = challenge[i];
}
for (i = 0; i < 15; i++)
{
auth_plain[i + 16] = uid[i];
}

stat = CSEC_DRV_GenerateMAC(CSEC_RAM_KEY, auth_plain, 248U, auth, 1U);
if (stat != STATUS_SUCCESS)
{
return stat;
}

stat = CSEC_DRV_DbgAuth(auth);
if (stat != STATUS_SUCCESS)
{
return stat;
}

return stat;
}

 

0 Kudos
Reply

2,280 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @wang_q4,

According to this thread of yours, you have already at least one key protected.

https://community.nxp.com/t5/S32K/CSEs-failed-to-restore-factory-Settings/m-p/1307273#M11340

In this case, it can be erased, unfortunately.

 

Regards,

Daniel

0 Kudos
Reply