How to measure the power mode transition time?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to measure the power mode transition time?

960件の閲覧回数
PYGC
Contributor II

PYGC_0-1676963782570.png

My measurements are larger than the DS results.

  • STOP1->RUN: 0.175us > (0.08us)
  • STOP2->RUN: 0.167us > (0.08us)

 

PYGC_1-1676964302694.pngPYGC_2-1676964351225.png

yellow: wakeup key

blue: core clock

0 件の賞賛
返信
3 返答(返信)

942件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @PYGC,

All specifications in Table 11 assume the clock configuration in Table 10.

Also, if you use an input active rising edge as a wakeup source, the port detects Vih_min at (0.65 x VDD), providing the input digital filter is not active.

 

Regards,

Daniel

 

 

 

 

0 件の賞賛
返信

926件の閲覧回数
PYGC
Contributor II

Is my measuring method correct? The start is VDD * 0.65, and the end is that the core clock has output.

0 件の賞賛
返信

918件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @PYGC,

What is the frequency of the core clock?

At 48MHz, one cycle is just 20ns.

The error if measurement can be significant.

What is the background of the query?

 

Regards,

Daniel

0 件の賞賛
返信