How to integrate SCST library with existing code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to integrate SCST library with existing code?

2,122 Views
sahyadriholagun
Contributor II

Hello,

I am trying to integrate the SCST library into our existing project.

The project is designed to run on a custom board with the S32K144 controller.

The project is built using GHS Compiler for ARM v2017.5.4.

When I execute the core self tests using the m4_scst_execute_core_tests() function, the function returns with M4_SCST_WRONG_RANGE. After executing a few lines of code following the m4_scst_execute_core_tests()  function call I get a hard fault.

I was able to execute the scst example code on our custom board without issue. I get the above results only after integrating with our existing project.

Please let me know how to debug this issue.

Tags (2)
0 Kudos
Reply
1 Reply

1,752 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

in this case, it would be better to create a ticket:

http://nxpcommunity.force.com/community/CommunityContextPage 

Thanks,

Lukas

0 Kudos
Reply