How to flash S32K144 using FreeMASTER?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash S32K144 using FreeMASTER?

3,802件の閲覧回数
hemantsindkar
Contributor III

Hi,

How to flash S32K144 using FreeMASTER S-Record transfer? Anyone is having flash driver files or procedure please share.

Thanks in advance.

Regards

Hemant

0 件の賞賛
返信
4 返答(返信)

3,254件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

the FreeeMASTER does not support this feature for S32K device.

As an aditional info you can look at AN4860 describing this feature for DSCs.  www.nxp.com/doc/AN4860

Unfortunately, DSC devices are the only which are supported by this feature.

The info is confirmed by FM design team.

Best regards,

Ladislav

0 件の賞賛
返信

3,254件の閲覧回数
hemantsindkar
Contributor III

Hi,

Which tool supports *.elf file flashing S32K144 without S32DS project or source code?

Regards

Hemant

0 件の賞賛
返信

3,254件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Hemant,

Which debug probe do you have?

One option is to use S32 Design Studio HOWTO: download separate elf/srec file to microcontroller using S32 Design Studio 

If you don't want to use S32DS you can e.g. use RAppID Bootloader but it supports just srec and not .elf loading

Overview of RAppID Bootloader|NXP 

Hope it helps.

Stan

0 件の賞賛
返信

3,254件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

probably you could go to the pemicro.com pages and search for cyclone, or use this link.

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

and search for S32 keyword.

Best regards,

Ladislav

0 件の賞賛
返信