How to flash S32K controller using EVAL board and Design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash S32K controller using EVAL board and Design studio

ソリューションへジャンプ
1,905件の閲覧回数
mayureshp
Contributor II
I have ECU with S32K144 controller on it. there is SWD connector on ECU. I want to flash this controller with S32K Eval board using S32KDesign studio. How can i do that? can i connect J14 of eval board directly to by SWD interface or is there any other connection required? What settings needs to be done on Design studio?
0 件の賞賛
返信
1 解決策
1,896件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi mayureshp,

I think you need to remove the R122 and R127 which connect the J14 to onboard S32K144.

debug interface R122 R127.png

But I suggest you take a look at this discussion: Program/Debug issue with S32K142-Q48

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,897件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi mayureshp,

I think you need to remove the R122 and R127 which connect the J14 to onboard S32K144.

debug interface R122 R127.png

But I suggest you take a look at this discussion: Program/Debug issue with S32K142-Q48

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信