How to find the S32K3xx FreeRTOS TCP/IP stack driver and example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to find the S32K3xx FreeRTOS TCP/IP stack driver and example

4,058 次查看
cranes
Contributor III

Hello,

Is there valid S32K3xx FreeRTOS TCP/IP stack driver and example available?

I downloaded all below installations and still failed to install any one of them.

cranes_0-1701657828792.png

There is a post https://community.nxp.com/t5/S32K/tcpip-1-0-3-can-t-be-installed/m-p/1686564#M25052 talking about this issue. But both two files mentioned in the post  S32K396_updatesize.zip and SW32K396_S32DS_3.5.1_D2207.zip can't be found any more.

Thanks!

Crane

 

0 项奖励
回复
10 回复数

4,041 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try this link; https://nxp.flexnetoperations.com/control/frse/download?element=13661857

Or go through Automotive SW - S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio -> click to Previous tab -> find S32 Design Studio Service Pack 1 EAR 1 with support for S32K396 devices 

BR, Petr

0 项奖励
回复

4,024 次查看
cranes
Contributor III

Thanks PetrS!

I do find the file and installed the S32K396 development package and RTD ver 3.0.0 successfully.

But how to find the TCP/IP stack? Checked the example available, and found two ethernet loopback examples. Is it in there?

Thanks!

Crane 

0 项奖励
回复

4,011 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check installation folder, if it really includes this stack. Examples are there...

PetrS_0-1701848785895.png

you can create new project from example within S32DS

PetrS_1-1701848930504.png

BR, Petr

0 项奖励
回复

3,993 次查看
cranes
Contributor III

Hello PetrS,

This is what I see in my folder after installing SW32K396_S32DS_3.5.1_D2207.zip:

cranes_0-1701915511876.png

In the PlatformSDK_S32K3 folder, only RTD, there is no stack folder.

These are what's installed:

cranes_1-1701915842680.png

When creating the project from the example, only RTD, no TCP/IP stack.

Anything might be missed in my installation?

Regards,

Crane

 

0 项奖励
回复

3,986 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

so if you now add/install tcpip stack, will it pass without any error popped out and appears within install folder?

BR, Petr

0 项奖励
回复

3,968 次查看
cranes
Contributor III

Hi PetrS,

Only S32K396_TCPIP_RTM_1_0_2_CD01_D2208_updatesite.zip adds it to the available software. And it requires FreeRTOS. 

When installing SW32K396_FreeRTOS_10_4_6_UOS_0_8_0_DS_updatesite_D2208.zip, I got this error:

cranes_0-1701995960925.png

But RTD S32K3xx v3.0.0 is already installed.

cranes_2-1701996066628.png

What might be still missing?

Thanks!

Crane

 

0 项奖励
回复

3,866 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

the FreeRTOS for S32K396 requires particular version of RTD. Based on FreeRTOS for S32K396 release notes the required RTD version is Code Drop 02 and S32K396 dev package EAR2:

jiri_kral_0-1702901181045.png

With this configuration you should be able install FreeRTOS package. 

0 项奖励
回复

3,862 次查看
cranes
Contributor III

Hello,

Ok got it. Thank you!

For RTD, I can only find these versions and couldn't find the version mentioned in your reply.

cranes_0-1702924120265.png

cranes_2-1702924387903.png

cranes_1-1702924327076.png

It happened before with another file as described in my another post. Is there anything missing in my searching or it indeed doesn't exist any more?

Thanks!

Crane

0 项奖励
回复

3,853 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to check "Previous" tab as well

PetrS_0-1702987349745.png

BR, Petr

0 项奖励
回复

3,847 次查看
cranes
Contributor III

Hello,

This is really weird. This is what I see in the previous tab:

cranes_0-1703000125361.png

Thanks!

Crane

 

0 项奖励
回复