How to find basic led blink example without RTD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to find basic led blink example without RTD

2,551 次查看
batuhanarslan
Contributor I

Hello,

I am a newbie to understand NXP environment for developing some of the projects. I wonder I added some packages on IDE. I can't see normal S32K1xx examples like S32K3xx Examples.

 

How can reach to them?

 

Kind Regards,

0 项奖励
回复
3 回复数

2,523 次查看
IsaulO
NXP Employee
NXP Employee

Hi @batuhanarslan ,

This S32K3xx Examples folder comes with the S32K3xx Development Package and only has one S32K358 example for estimate PI using the Monte Carlo approach.

Untitled picture.png

If you are looking for examples for the S32K1xx without using RTD you can find some in the following path: S32K1 page >> Documentation >> AN4513: S32K1xx Series Cookbook

Untitled picture1.png

Note: These example projects are implemented using NXP’s S32 Design Studio v 3.3, for newer S32DS versions we recommend using RTDs, such as RTD 2.0.0 


BR,
IsaulO.

0 项奖励
回复

2,518 次查看
batuhanarslan
Contributor I

Hi @IsaulO ,

Thank you for your response. I also wonder is any  document or blog I follow a understanding basic pin configurations?

Best regards,

0 项奖励
回复

2,459 次查看
IsaulO
NXP Employee
NXP Employee

Regarding pins configuration you can check all the possible configurations for each pin in the Pins configuration tools section in your S32DS IDE, as you can see in the following image:

Untitled picture1.png

Additionally, you can refer to the attached S32K1xx_IO_Signal_Description_Input_Multiplexing.xlsx files in the Reference Manual for the Pinout for your specific controller.
S32K1xx MCU Family - Reference Manual

Sign in is required to obtain the reference manual.

BR,
IsaulO.

 

0 项奖励
回复