How to determine the reset cause between external pin reset and internal reset on the S32K

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to determine the reset cause between external pin reset and internal reset on the S32K

2,149 次查看
Hozumi
Contributor I

How to determine the reset cause between external pin reset and internal reset on the S32K?

During the internal reset, the reset pin was set to low for about 500 us.

In the case of an external pin reset, how long should the reset pin be set to low?

0 项奖励
回复
3 回复数

2,143 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Ken3,

Each reset source has an associated field in the Reset Control Module (RCM) System Reset Status (RCM_SRS) register.
You can check the vaule of RCM_SRS.

25.2 Reset.png

Best Regards,
Robin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,137 次查看
Hozumi
Contributor I

Hi Robin,

 

Thank you for your reply.

Is there a min-max specification for the length of the Low signal applied to the reset pin during power on?

0 项奖励
回复

2,129 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I only find this: WNFRST is the recommended external reset low pulse Min.

WNFRST.png

0 项奖励
回复