How to compile the entire SDK in IAR Workbench

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to compile the entire SDK in IAR Workbench

3,021 Views
geoff_ar
Contributor I

Is there SDK available which is IAR  toolchain compatible.

Controller used is S32K142.

Current SDK package used is S32_SDK_S32K1xx_RTM_4.0.0

0 Kudos
Reply
3 Replies

2,922 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

From the release note of the S32_SDK_S32K1xx_RTM_4.0.0 can be seen information below:

pastedImage_1.png

So, S32 SDK supports IAR v 8.11.2

Best regards,

Diana

0 Kudos
Reply

2,922 Views
geoff_ar
Contributor I

Hello Diana,

Release notes states that it is compatible. However, when i tried to compile it's giving error. The error comes due to some piece of code in the project. Moreover, project settings file for IAR toolchain is not present in SDK.

Is there any way by which i can get the project file(.ewp) for examples present in sDK.

Thanks and Regards,

Geoff Aabel Roy

0 Kudos
Reply

2,922 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Geoff,

I'm not sure, in which S32DS do you use the IAR toolchain?

There is "hello_world_iar" which includes .ewp file located here:

C:\NXP\S32_SDK_S32K1xx_RTM_4.0.0\examples\S32K148\demo_apps\hello_world_iar

I hope it helps.

Best regards,

Diana

0 Kudos
Reply